Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
If my circuit monitor series 2000 has firmware version 14 or below can I upgrade it with DLF to the latest firmware version?

Product Line
CM2000
DLF-3000

Environment
Firmware Upgrade

Resolution
Yes, see FA237920 for steps on how to upgrade the firmware. Make sure you backup the data logs and note the CT and PT settings and other general configuration settings. This information could be lost when performing the firmware upgrade.