Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to automatically restart a PME service that has failed
Issue
How to automatically restart a service that has failed

Product Line
PME, ION Enterprise

Environment
Windows Services

Cause
Services may require restart when they have failed.

Resolution
The service can be configured to automatically restart:

  1. Open Windows Services
  2. Right-click lmadminSchneider
  3. Go to Properties
Services screen
  1. Open the Recovery tab
SQL Server Agent
  1. Configure service to restart after first and second failure