Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ADDENDUM TO 3710 ACM - INSTALLATION AND OPERATION MANUAL P24/48 OPTION

Product Line:
3710 ACM

Environment:
Addendum to the Installation and Operation Manual

Resolution:
The Addendum to the 3710 ACM Installation and Operation Manual P24/48 Option contains:
____________________________________________________________________________
3710 ACM Addendum: P24/48 VDC Power Supply Option Power Measurement Ltd.

ADDENDUM TO 3710 ACM
INSTALLATION AND OPERATION MANUAL

P24/48 OPTION

92/6/12


WARNING
THE UNIT CONTAINED WITHIN IS SPECIALLY
DESIGNED TO OPERATE FROM 24 OR 48 VOLT D.C.

APPLICATION OF A.C. VOLTAGE TO THE "POWER" INPUT
TERMINALS WILL PERMANENTLY DAMAGE THE UNIT AND
VOID THE WARRANTY.

DO NOT HIPOT TEST THE POWER INPUT TERMINALS OF THIS UNIT.

POWER SUPPLY WIRING
Positive D.C. Voltage Wire: 3710 ACM "L" Terminal.
Negative D.C. Voltage Wire: 3710 ACM "N" Terminal.
______________________________________________________________________________
Please see attached .pdf for the official release.

*The Installation and Operation Manual can be found in FA212861

Schneider Electric Saudi Arabia

Attachment(s)
ADDENDUM_TO_3710_ACM_INSTALLATION_AND_OPERATION_MANUAL_P24_48_OPTION.pdf [12.15 KB]