Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
PM 600 series Modbus Register List

Issue
Power meter 600 series modbus register list is required

Product Line
PM 600 series meter

Environment
PM 600 Series meter register read/write

Cause
Documentation of modbus register list is needed for the PM 600 series meter.

Resolution
Modbus Register list for PM 600 series meter is attached along this article.

Schneider Electric Saudi Arabia

Attachment(s)
PM_600_Modbus_list.pdf [93.33 KB]