Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the split core current transformer (CT) cables be extended on the Split-Core Branch Current Monitor (BCMSC) meter?

Issue:
The end user would like to extend the length of cables attached the a Current Transformer on a BCMSC meter.

Product Line:
Branch Current Monitor Split Core (BCMSC)

Environment:
Current Transformer for BCMSC

Cause:
The monitoring source may be beyond reach of the Current Transformer that comes standard with the BCMSC.

Resolution:
The split core current transformers can be extended to a maximum distance of 20 feet. The recommended wire size is 10 gauge (AWG).