Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
171CCC9x0x0 M1E Processor 984LL Exec. Upgrade to v.1.25

Issue
The purpose of this resolution is to inform Momentum M1E users that the 984LL Exec. has been upgraded to version 1.25.

Exec. v.1.25 resolves an issue with pinging an M1E through a router across a WAN. This problem occurred in 984LL Exec. versions 1.21 and 1.23. It did not occur in v.1.20.


Product Line
· 171CCC98030
· 171CCC96030
· 171CCC98020
· 171CCC96020



Resolution
Installing 984LL Exec. v.1.25 resolves the above-mentioned issue.

Note: It is recommended to power cycle the M1E immediately after downloading an Exec.


Legacy KB System (APS) Data: RESL174643 V2.0, Originally authored by on , Last Edited by on
Related ranges: Modicon Momentum

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre