Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Momentum M1 IEC Exec. Upgrade to v.2.11e

Issue
The purpose of this resolution is to inform Momentum product users that the IEC Executive firmware for M1 processors has been upgraded to v.2.11.


Product Line
Momentum


Resolution
IEC Exec version 2.11 resolves the following issues:
1) M1 IEC Exec version 2.11 did not allow OFS to access Concept IEC unlocated variables.
2) An xxmit Function Block in an M1 Processor may fault with an error 150 (in the xxmit block) if the xxmit block is active (powered) when the PLC is power cycled.


Installing IEC Exec. v.2.11 resolves the above-mentioned issues.


Legacy KB System (APS) Data: RESL192572 V1.0, Originally authored by DaDz on 08/23/2008, Last Edited by DaDz on 08/23/2008
Related ranges: Modicon Momentum