Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to find the amount of free memory in the SD card for the BMXNOE0110.

Issue
How to find the amount of free memory in the SD card for the BMXNOE0110.

Product Line
BMX NOE 0110

Environment
Web Designer

Resolution
To see the amount of free memory,

  • Start Web Desginer.
  • Open the Web Designer application.
  • Click on the target name (i.e., BMX NOE 0110 - Target 0 ...)
  • Click on Target from the top menu.
  • Click on Site Explorer .
  • Click on the IP address for the target in the Site Explorer View tab.
  • The free memory in the SD card will be shown on the bottom left of the site explorer window.