Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Web Reporter report packs and RS will not install on Windows XP SP3 machine

1) Check to that the ASPNET User account has been created

To do this, click Start > Control Panel > Administrative Tools > Computer Management.


  • 2) Expand Local Users and Groups and click the Users folder

NOTE: ASPNET does not always install properly on Windows XP SP3, so the user account may not be created. SQL Server requires that the ASPNET account exists so that Reporting Services can be installed properly during installation. ION Enterprise Web Reporter will not function as expected if Reporting Services has not been installed properly.


  • 3) If the ASPNET account doesnt exist, it must be reinstalled before installing SQL Server and ION Enterprise. This step may be skipped if the ASPNET user account exists.

      • Open Command Prompt: Start > Run > Type "cmd"

        Go to c:\windows\microsoft.net\framework\v2.0.50727>

        Run the command "aspnet_regiis -i"

        Run the command "iisreset" to restart IIS



    4) Check that the ASPNET account was created (refresh the view)

Legacy KB System (APS) Data: RESL201266 V1.0, Originally authored by CoBu on 02/03/2010, Last Edited by CoBu on 02/03/2010
Related ranges: ION Enterprise V6.0

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre