Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Short Circuit Current Ratings (SCCR) and branch circuit protection Recommended fuse ratings for UL and CSA requirements for ATV212 driveline

Issue:
Looking for a circuit breaker or fuse that is used with the ATV212 drive.

Product line:
Altivar 212

Environment:
All models, all serial numbers

Cause:
Recommended fuse rating for UL and CSA requirements.

Resolution:
The breaker and fuse sizing can be found in the ATV212 Quick Start Annex.

ATV212 Quick Start Annex (SCCR and Branch Circuit Protection) | Schneider Electric

“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Saudi Arabia

Attachment(s)
ATV212 Annex.pdf [106.95 KB]