Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the buttons on the faceplate of the ATV212 and ATV21 be disabled?
Issue:
Disable the keys on the faceplate of the ATV212 and ATV21.

Product line:
Altivar 21/212

Environment:
All models, all serial numbers

Cause:
How to disable the functionality of the buttons on the faceplate of the ATV21/212?

Resolution:
Press mode button to AUF
Press down arrow to F--- Press enter
Press down arrow to F730 (Up/down key reference) set to 1 (disable) press enter
Press down arrow to F732 (Loc/Rem key) set to 1 (disable) press enter
Press down arrow to F733 (Run/Stop key) set to 1 (disable) press enter
Press down arrow to F734 (Priority stop) set to 1 (disable) press enter
Press down arrow to F735 (HMI reset button) set to 1 (disable) press enter