Issue:
Customer is in need of accessories for AR3100X717 or AR3104X717.
Product Line:
NetShelter Dell OEM
Environment:
All versions and serial ranges.
Cause:
Need to identify compatible accessories.
Resolution:
All accessories that are compatible with AR3100 and AR3104 also compatible with AR3100X717 and AR3104X717 with one exception AR7719, Castor Kit. For a list of the available accessories please see the NetShelter Accessory Compatibility Chart which is available from the Knowledge Base on the APC website. Please search for document FA158651: http://www.apc.com/site/support/index.cfm/faq/
Released for:Schneider Electric Saudi Arabia