Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
In Vijeo Designer, can I access the properties of the Numeric Display object to lock-out or allow the input mode from scripting?

Issue
In Vijeo Designer, can I access the properties of the Numeric Display object to lock-out or allow  the input mode from scripting?

Product Line
Vijeo Designer

Environment
HMI Programming Software

Resolution
No, there are no scripting methods that will allow you to lock-out or allow  the input mode of the numeric display object.  A work-around would be to use the Security feature and set a Security Level for the numeric display object, or set Visibility on an Rectangle with Invisible Colour drawn on top of the Numeric Display.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)