Issue:
Part number for ATV312 Din rail mounting kit
Product Line:
ATV312
Environment:
All
Cause:
Desire to utilize din mounting kit option
Resolution:
The part numbers need to order the mounting kit for this drive are VW3A9804 and VW3A9805.
VW3A9804 covers the following range of drives: ATV312....
018M2, H037M2, H055M2, H075M2, H018M3, H037M3, H055M3, H075M3
VW3A9805 covers the following range of drives: ATV312....
HU11M2, HU15M2, HU11M3, HU15M3, HU22M3, H037N4, H055N4, H075N4, HU11N4, HU15N4, H075S6, HU15S6
Note: The din rail mounting kits are only available for the above drives.
Note: Other drives not list above do not have a din rail kit.
Part number for ATV312 Din rail mounting kit
Product Line:
ATV312
Environment:
All
Cause:
Desire to utilize din mounting kit option
Resolution:
The part numbers need to order the mounting kit for this drive are VW3A9804 and VW3A9805.
VW3A9804 covers the following range of drives: ATV312....
018M2, H037M2, H055M2, H075M2, H018M3, H037M3, H055M3, H075M3
VW3A9805 covers the following range of drives: ATV312....
HU11M2, HU15M2, HU11M3, HU15M3, HU22M3, H037N4, H055N4, H075N4, HU11N4, HU15N4, H075S6, HU15S6
Note: The din rail mounting kits are only available for the above drives.
Note: Other drives not list above do not have a din rail kit.
Released for:Schneider Electric Saudi Arabia