Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there tech support or drivers available for APC-4902, USB1284 or 19008?

Issue:
Technical support is required.

Product Line:
Cables and Connectivity Solutions

Environment:
USB to Parallel, USB Extension, USB to IEEE1284

Cause:
Need drivers or other technical support.

Resolution:
The APC-4902, USB1284 and 19008 are all 'plug-n-play.' They do not require drivers.

For technical support on APC-4092, USB1284 or 19008 please contact APC Cables.
Phone: 888-370-6688 in North America
email: support@apccables.com