{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
G3200: Why are the upperBound and lowerBound for Modbus registers not behaving as expected?

If RegisterType is m/M, then optional field for scaling and offset looks like

size:scale:[lowerBound:]upperBound;O:offset

The lowerBound and upperBound must be entered in hexadecimal format.

For more information on optional fields, refer to the PowerLogic G3200 Modbus-to-IEC 61850 Server User's Manual, PLSED309028EN.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.