Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where can I find the FO (Factory Order) or Q2C number for an E-Flex drive?
Issue:
FO (Factory Order) or Q2C number for an E-Flex drive.

Product Line:
Enclosed Altivar 61, Enclosed ATV61, E-Flex, Eflex

Environment:
All models

Cause:
To determine warranty status or check the Bill of Materials for spare parts.

Resolution:
On the back of the E-Flex enclosure door is the nameplate.  At the bottom of the nameplate, you will see "Made in USA" or "Made in Mexico".  The second box is a two digit plant code.  The third box is an 11 digit number which is our Factory Order/Q2C number.

Schneider Electric Saudi Arabia

Attachment(s)
E-Flex nameplate.jpg [172.98 KB]