Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the maximum humidity acceptable with the Altivar ATV61 and 71 drives?

Issue:
Maximum humidity acceptable with the Altivar ATV61 and 71 drives.

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
humidity

Resolution:
95% maximum without condensation or dripping water.