Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
For the Enclosed ATS22, what is the difference between the Basic Shunt Trip and Full-Featured Shunt Trip power circuit options?

Issue:
What is the difference between the Basic Shunt Trip and Full-Featured Shunt Trip versions of the Enclosed ATS22?

Product Line:
Enclosed AST22

Environment:
All models

Cause:
Define features for quoting

Resolution:
The electrical schematics are the same.  The Basic Shunt Trip unit is a space optimized version of the Enclosed 22 controller.  Limited space is provided for field mountable control equipment.  The Full-Featured Shunt Trip unit is a fully customizable version.  Additional space is provided for engineered options and field installable equipment.