Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to import a PS1131 Codesys program for an ATV-CI Controller Inside card into SoMachine 3.1 for an ATV-IMC Drive Controller card?
Title
PS1131 Codesys program for ATV-CI Controller Inside card, question about migration to SoMachine 3.1.
Issue
A customer is trying  to import a PS1131 Codesys program for an ATV-CI Controller Inside card into SoMachine 3.1 for an ATV-IMC Drive Controller card.
Product Line
ATV-CI Controller Inside card, ATV-IMC Drive Controller card
Environment
PS1131 software, SoMachine 3.1 software
Cause
PS1131 and SoMachine 3.1 are based on different Codesys versions.
Resolution
There is no automatic conversion from ATV-CI to ATV-IMC available.Also, the libraries for ATV-CI are not compatible with ATV-IMC libraries.


If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)