Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How is the Estimated motor torque value calculated on the ATV212?

Issue:
With the analog signal FnSL set at 7, estimated motor torque, how can you tell what the scaling of the analog output is?

80378765
ATV212, Altivar 212, S-Flex

Environment:
Altivar

Cause:
Customer needs to know what the scaling factors are.

Resolution:
The base torque value is calculated from the drive HP size and setting of parameter F417 (Rated motor Speed or RPM).
The calculation is Motor HP * 5250 / RPM.

For example, a 10HP drive with 1750RPM.  10*5250/1750 = 20lb-ft or torque.
This means that 100% of the estimated torque is 20 lb-ft.
Since the scaling of the analog output when set to torque is 0-250% of the rated motor torque, the analog output will be scaled 0 to 50 lb-ft.

“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)