Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What does the Z suffix mean on the ATV61 and ATV71 drives?

Issue:
Z suffix meaning on ATV61/71.

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
What is the difference between the non Z suffix and Z suffix ATV61 and ATV71 drives?

Resolution:
The Z suffix means the ATV61 or ATV71 drive, will ship without the VW3A1101 graphics keypad display.