Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the ATS22 remote keypad?

Article available in these languages: Czech, Spanish

Issue:
What is the remote keypad for the ATS22?

Product Line:
Altistart 22 ATS22

Environment:
All models

Cause:
Keypad interface to be remote from ATS22.

Resolution:
The accessory remote keypad options are:
VW3G22101 for IP54 / Nema 12
VW3G22102 for IP65

Cable options to connect the keypad to the ATS22 are (sold separately):
VW3A1104R10 for 1 meter length
VW3A1104R30 for 3 meter length