Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: How do you remove the main control board on the ATV61/71 drives?

Issue:
Removing the main control board on the ATV61/71 drives.

Product Line:
Altivar ATV61/71 drives

Environment:
All

Cause:
Needs to understand how to remove and reinstall the MCB on the ATV61 and ATV71 drives

Resolution:
The document number for the Instruction Bulletin on the ATV61/71 Control Board Kits is 30072-451-86A (attached below).

Schneider Electric Saudi Arabia

Attachment(s)
30072-451-86A.pdf [706.19 KB]