Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Webreach Displays an Objects caption in Purple
Issue:
A user observes that some of the captions in Webreach or Web Applications 'Diagrams' are purple, while others match the caption color set in Vista.
Product Line:
ION Enterprise 6.0.x
Struxureware Power Monitoring 7.0.x  (SPM 7)
Environment:
Webreach in Internet Explorer 8. (May affect other versions of IE as well)
Cause:
If the objects in Webreach  or Web Applications 'Diagrams' have actions associated with them (Example: they open another diagram) Internet Explorer will recognize this as a link. When the customer clicks the link, Internet Explorer treats this as a visited link.
Resolution (Workaround):
In Internet Explorer, navigate to Tools> Internet Options.
On the General tab, under the 'Appearance' heading click "Color".
Uncheck "Use Windows Colors" then can change the color of the "Visited" links to match the caption color set in Vista.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre