Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
WSOS V5 crashes after installation
Issue
When WSOS is double clicked, the application crashes with the error:

Stopped Working


Application Event Viewer

Environment
Windows 7 64 bit OR 32 bit

Cause
The application crashes due to missing MSXML package

Resolution
The software requires that MSXML 4.0 Service Pack 3 be installed on the system

Below is a link to download the compatible version of MSXML from Microsft's website:
https://www.microsoft.com/en-us/download/details.aspx?id=36292