Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the ATS48 Soft Starter be programmed to run a motor in reverse?

Article available in these languages: Spanish

Issue:
Can the ATS48 Soft Starter be programmed for reverse?

Product Line:
ATS48

Environment:
All serial numbers for ATS48

Cause:
N/A

Resolution:
No, the ATS48 Soft Starter cannot be programmed for reverse.  If a reverse option is required, use a reversing contactor ahead of the ATS48. Please see Figure 35 in the attached manual for a diagram.

Schneider Electric Saudi Arabia

Attachment(s)
S1A37491.pdf [1.3 MB]