Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the VW3A1101 keypad be swapped between ATV61 and ATV71 drives?
Issue:
Can the HMI display be swapped between ATV61 and ATV71 drives?

Product Line:
Altivar ATV61  ATV71

Resolution:
Yes, the VW3A1101 keypad is common to both ATV61 and ATV71 product lines and is interchangeable between them. To prevent an HMI comm fault/error when disconnecting the HMI, ensure that the drive is not in local control (being controlled by the HMI).  To prevent this fault, the drive needs to be in terminal or communications control.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)