Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the thermal sensor on a ATV61 or 71HD30N4?
Issue:
ATV61 or ATV71HD30N4 thermal sensor part number

Product Line:
ATV61 ATV71

Environment:
ATV61HD30N4 ATV71HD30N4

Cause:
Replacement thermal sensor

Resolution:
The ATV61 / 71HD30N3 thermal sensor is a VZ3G1101