Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Power Monitoring Expert - When I try to navigate to a device in Diagrams, I am told 'the template for the requested device cannot be found' even though it works in Vista

Issue
User sees the message "The template for the requested device cannot be found" when attempting to go to a device's default template page in Diagrams even though the same thing works in Vista.

Product Line

Power Monitoring Expert 7.2.x

Power Monitoring Expert 8.x

Power Monitoring Expert 9.0

Power Monitoring Expert 2020

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023


Environment
PME Web Applications

Resolution
The Diagrams Web Application can have a problem using auto-diagram to open a device diagram if the device name contains unusual but permitted characters.

As an example, consider a device with the name 'testau)to-r+ep=or(ter!na#m$e&'.

These types of unusual characters cause problems in a web environment because they become part of the URL and are not interpreted correctly in a web browser. The workaround is not to use these types of characters in device names.