Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where are wiring diagrams for an ATS22 Enclosed softstart?

Issue:
Looking for a wiring diagram for an ATS22 enclosed softstart.

Product Line:
Enclosed 22  863922U  863822U

Environment:
All

Cause:
NA

Resolution:
If order specific drawings are not available, power circuit diagrams and many example control diagrams are found in the Enclosed Altistart 22 Instruction bulletin, number 30072-453-26, available at https://www.se.com/us/en/download/