Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the tbS setting and status on an ATS48 soft start?
Issue:
TBS function on the ATS48 softstart

Product Line:
Altistart 48, ATS48

Environment:
All models and serial numbers

Resolution:
This parameter avoids starts in quick succession which may overheat the motor. The time delay starts when the motor changes to freewheel mode.
In 2-wire control, the motor is restarted after the time delay if the RUN command input is still activated.
In 3-wire control, the motor is restarted after the time delay if a new RUN command is sent (rising edge).

The soft starter displays "tbS" during the time delay.
If tbS displays unexpectedly, check the  start/run circuit.