Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Please confirm that RA1GA75105 is not in production anymore?

The RA1GA*** are out of production since several years (>10). The RA1GA75105 was a three phase thermal relay for setting between 75 and 105A. You can replace it by a LR9G115 from 28 to 115A or LR9G225 from 57 to 225A.

Schneider Electric Saudi Arabia

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: