Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are DC chokes available as a spare part on ATV61 and ATV71 drives?

Issue:
DC Choke availability for ATV61 and ATV71 drives.

Product Line:
ATV61 and ATV71

Environment:
All models and serial numbers

Cause:
None

Resolution:
DC Chokes are not in our offering for spare parts on the Frame sizes 2 thru 8.
DC Chokes are offered as replacement parts only on some of the Frame sizes 9 thru 15.
Contact the Drives Product Support Group for assistance 1-888 778 2733.