Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for Line reactors for ATV drives in the Canadian market?

Issue:
Altivar drives line reactor part numbers.

Product Line:
ATV12, ATV312, ATV61, ATV71

Environment:
Canadian Market

Cause:
3% Line reactors.
5% Line reactors.
Dv/Dt Filters

Resolution:
Please see attached sheet.
For ATV31,  use the ATV312 selection sheet.

Schneider Electric Saudi Arabia

Attachment(s)
ATV12-312-61-71_Line and Load reactors and dv-dt Filters.xls [128.5 KB]