Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why is the numeric display object input ranges are 0 for the min and max in Vijeo Designer simulator and runtime?
Issue
In Vijeo Designer Simulation Mode or Runtime, why are the Numeric Display object input ranges shown as 0 for the Min and Max in the Numeric Value Entry keypad?

Product Line
Vijeo Designer

Environment
HMI Runtime and HMI Simulation Mode

Cause
If the variable is a Real (Floating Point) and the Numeric Display object was setup as an Integer data type, the Min and Max will appear as 0.

Resolution
Change the Data Type radio selector in the Numeric Display object from "Integer" to "Float" to represent the "Real" Data Type of the actual Variable.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)