Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What communication options are available on the ATV12
Issue:
What communication options are available on the ATV12?

Product Line:
ATV12

Environment:
ATV12

Cause:
Network communications options

Resolution:
The ATV12 only has the modbus communication protocol available.   A third party gateway can be used for other protocol of customer's choice.