Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
In programming PID, what does parameter FbS do on an ATV312 drive?
Issue:
Parameter FbS (feedback scale factor)

Product Line:
ATV31 and ATV312

Environment:
All models and serial numbers

Cause:
None

Resolution:
The parameter FbS is a parameter that can be used to scale the reference according to the range of the feedback sensor.
Example: Regulating pressure
PI reference range of process, 0-50 psi (0-100%)
Range of pressure sensor, 0-100 psi
FbS = Max sensor range / Max process range
FbS = 100/50 = 2