Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: How to arrange devices and sites alphabetically in ION Setup?
Issue
A user wants to arrange 'Sites' and 'devices' alphabetically in ION Setup.

Product Line
ION setup 3.0

Environment
Network Mode in ION Setup

Cause
ION Setup arranges sites and devices in the order they were introduced: the oldest device or site appears at the top, the newest at the bottom.

Resolution
From the Menu bar of ION Setup in Network View mode select "Tools>Options>View> (check the box next to)Sort Network Items>OK"

Close and then reopen ION Setup. Sites and devices are now alphabetically arranged.