Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the OPC server name for PME?
Issue
The OPC server name is required in order to connect to the Power Monitoring Expert OPC server.

Product Line
ION Enterprise 6.0.x
StruxureWare Power Monitoring 7.0.x
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.x
Power Monitoring Expert 9.x
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023

Environment
Power Monitoring Expert as an OPC server

Cause
The name of the PME OPC server is unknown.

Resolution
The name of the OPC server isION.OPCDAServer as shown below:


OPC Test Client