Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can a logic input be used as a scope trigger in SoMove?
Issue:
SoMove O-scope trigger function

Product Line:
ATV12, ATV312, ATV32, ATV61, ATV71, ATS22, ATS48, ATV320, ATV340, ATV630, ATV930

Envoronment:
All Serial numbers

Cause:
None

Resolution:
Logic inputs can be used as a scope trigger in SoMove V2.6.

Schneider Electric Saudi Arabia

Attachment(s)
Capture.PNG.png [61.93 KB]