Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Vista - Changing Dial Display Range and Ticks

Issue
User wants to change range and tick marks of the Full and Partial Dial Displays in Vista.

Product Line

Power Monitoring Expert 2024

Power Monitoring Expert 2023

Power Monitoring Expert 2022

Power Monitoring Expert 2021

Power Monitoring Expert 9.x

Power Monitoring Expert 8.x

Power Monitoring Expert 7.2.x


ION Enterprise
Struxureware Power Monotoring (SPM)

Environment
Configuring dial objects in Vista.

Cause
Dials are by default set to a range of 0 to 2000.

Resolution
1. Open Vista.exe and navigate to the desired diagram.
2. At the top, click options then make sure 'Show Toolbox' option is selected.
Vista Menu
3. Right click on the dial to open up the object configuration.

4. Click on the Display tab at the top and right click on the preview window at the bottom right.
Object Menu

5. On the Meter Parameters window, change the Range and Ticks to the preferred values and click Ok.
Object properties