Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How is the ATS48 acceleration ( ACC ) setting programmed?
Issue:
ACC parameter on a ATS48 soft start.

Product Line:
ATS48

Environment:
All

Cause:
Intend to change the time required to bring the motor to full speed.

Resolution:
Ensure that there is no start command.  ATS48 status display should be rdY or nLP.
On the ATS48 keypad, press the down arrow button to the SEt menu and press ENT.
From parameter In, press the down arrow multiple times to parameter ACC and press ENT.
Use the up / down arrow buttons to select the desired start time in seconds.
Press ENT to save the value.