Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which are the location where EPOXY COATING can be done on busbars in BlokSeT?
The epoxy coating reduces the risk of flash-over (arc) and protects the switchboard and operators against dropped tools, bolts, nuts etc.
  • For BlokSeT D, we use epoxy for horizontal and vertical busbar and for all the busbar connections with Masterpact, incoming and outgoing (except Joints).
  • For BloksSeT Mf, horizontal, vertical busbar, busbar connection between vertical busbar and NS / NSX / NSXm (line side)
  • For BlokSeT Ms and Blokset Dc, only the horozontal and VBB has to be coated with epoxy.
  • For BlokSeT Mw2 only HBB can be epoxy coated.