Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where can I get dimension drawings for the M-Flex enclosures?

Issue:
Could not find the schematics for M-flex

Product Line:
Altivar Machines, Altivar 71, M-flex

Environment:
All models and serial numbers

Cause:
N/A

Resolution:
The dimensions for the M-Flex enclosures can be found on page 33 - 46 of the M-Flex manual.
Catalog number is 30072-451-52

Schneider Electric Saudi Arabia

Attachment(s)
30072-451-52.pdf [2.2 MB]