Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can a Powerlogic or ION meter be used for monitoring Variable Frequency Drives (VFDs)?
Issue
Can the output of a VFD be measured using a Powerlogic or ION metering solution?

Product Line
Powerlogic Metering
ION Metering

Environment
Metering
Energy Management

Cause
Can ION or Powerlogic meters be used to monitor the output of a VFD for energy consumption and/or frequency monitoring.

Resolution
Powerlogic and ION metering families are not designed for non-sinusoidal variable frequency waveforms. These meters are designed to measure a fairly constant frequency, and have a very small range of variance (usually 45-65 Hz depending on the specific device). Because of this, they are unable to measure the output of a variable frequency drive.