Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is default IP address of a M221 PLC?

Article available in these languages: Japanese

The IP address by default is 10.10.x.x.
The last 2 fields in the default IP address are composed of the decimal equivalent of the last 2 hexadecimal bytes of the MAC address of the port.
The MAC address of the port can be retrieved on the label placed on the front side of the controller.
The default subnet mask is Default Class A Subnet Mask of 255.0.0.0.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)