Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What will cause enclose units not to run the motor in AFC or in Bypass?
Issue:
Enclosed units not to running the motor in AFC or in Bypass.

Product Line:
SFLEX, EFLEX, MFLEX, CPD, MCC, Field Drive, Econoflex, 58M

Environment :
All Enclosed products with Bypass

Cause:
The motor will not run in AFC or in Bypass

Resolution :
1).  Check supply fuse primary side of transformer.
2).  Check fuse on the secondary side of the transformer
3).  Verify the overload is not tripped, (trip and then reset)
4).  Verify the AFC/OFF/Bypass switch is getting voltage
5).  With factory drawing in hand check the HOA and the AFC/OFF/Bypass circuit.

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: