Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do the ATV61 and ATV71 Drives have a built in ON delay timer for the logic inputs?

Article available in these languages: Spanish

Issue:
Can a delay be added to the logic inputs on the ATV61 and ATV71 Drives?

Product line:
Altivar 61 & 71

Environment:
All models, all serial numbers.

Cause:
Customer needs to delay the run command after LI1 closes.

Resolution:
Using the HMI or keypad, under Menu 1.5 Inputs/Outputs CFG, go to LI1 Configuration and select LI1 On Delay.
The default setting for this parameter is 0ms, but can be set to 0 to 200ms.
The time delay function is available on all the logic inputs.