Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can I connect a Magelis HMISTU to a Zelio Smart relay?
The Magelis HMISTU (655/855) can communicate to a Zelio Smart relay via Modbus serial or Modbus/TCP (Ethernet).

For serial communication you would need the the following.
XBTZ9980 cable 2.5m or the ZBTZ9982 10m
SR3MBU01BD Zelio Modbus module

For Ethernet communication:
Ethernet cable
SR3NET01BD Zelio Ethernet module.

Both Zelio communication modules are compatible with the SR3B***BD smart relay only.